ROHM Device Manufacturing’s semiconductor devices are used across diverse sectors to meet needs for improved efficiency, energy conservation, and high breakdown voltage.
Our manufacturing quality plays an important role in reliably obtaining these properties.
We merge the technologies and know-how cultivated at each manufacturing site to simultaneously achieve improved quality and stable supply.
Through reliable manufacturing, we support the development of infrastructure and industry and help realize a sustainable world.
SiC power devices Silicon carbide (SiC) is a next-generation power semiconductor material that can be used in place of traditional silicon. Offering both high breakdown voltage and low loss, SiC delivers excellent performance in high-temperature environments and high-power applications.
LSIs
Large scale integrated circuits (LSIs) are ICs in which peripheral circuits required for CPUs, memories, and other electronic devices are integrated on a chip.
These products stand out for high breakdown voltage, helping improve the energy and operational efficiency of customers’ products.
LEDs
Light emitting diodes (LEDs) are semiconductor devices that convert electrical energy to light highly efficiently.
They feature long life and high reliability, contributing to energy conservation and the reduction of environmental burden in illumination and display applications.
Power transistors
Power transistors are semiconductor devices that can provide basic functions, such as signal amplification and switching, as a stand-alone device.
We offer a wide lineup of excellent low-power consumption, high-breakdown voltage, and high-reliability transistors, supporting diverse applications from consumer products to automotive and industrial equipment.
Diodes
Diodes are basic semiconductor devices that pass a current in one direction only.
We offer excellent low-loss, high-speed response, and high-reliability diodes, supporting the stable operation of all kinds of electronic devices, including the rectification and protection of power supply circuits.
GaN devices
GaN (gallium nitride) is a next-generation power semiconductor material.
Offering fast high-speed switching and low loss, GaN contributes to the downsizing and energy conservation of power supplies and communication devices for which high frequency and efficiency are required.
We contribute to society by flexibly addressing the diversifying needs of the electronics market, from consumer products to industrial equipment.

Automotive equipment Our automotive equipment supports the evolution of automotive technologies, including meter panels and illumination systems, as well as applications related to HEVs and EVs.

Industrial equipment We offer devices matching market needs in the industrial sector, such as energy conservation and downsizing, supporting technological innovation.

Information and communication devices These devices are widely used in products that are essential to modern life, including smartphones, smartwatches, and tablets.

Energy-related equipment This equipment is utilized in control technologies that are vital to renewable energy, such as wind and solar, helping realize decarbonization.
The ROHM Group is an integrated device manufacturer (IDM) that handles all stages of production, from development through manufacturing. ROHM Device Manufacturing Co., Ltd. is responsible for the front-end processes, ensuring the stable supply of high-quality products.

The wafer processing technologies in front-end processes are essential to the mass production of semiconductor devices, including LSIs and discrete products.
In wafer processing, the performance and quality of semiconductor devices are achieved through numerous micrometer- and nanometer-scale microfabrication and chemical treatment processes.
These processes are very complex, and even slight variations cannot be tolerated.
The ROHM Group has cultivated advanced device and processing technologies over many years. This gives us an advantage in SiC power devices and analog LSIs as well as discrete products, including transistors and diodes.
SiC power devices must stably operate in high temperature and high voltage environments; analog LSIs are necessary to improve the energy and operational efficiency of finished products; and high reliability is required for discrete products. For these devices and products, processing precision and reproducibility in front-end processes are important factors that determine product performance.
We realize high reproducibility and stable quality in mass production by optimizing our production facilities and processing technologies for each product’s applications and characteristics.
Based on our accumulated expertise in such technologies and facilities, we support the performance and reliability of semiconductor devices on the manufacturing side
as a global manufacturing leader, mainly in the automotive, industrial, and energy sectors.

Semiconductor manufacturing equipment specialized for complex and ultra-high-precision processing

Cutting-edge analytical equipment including focused ion beam scanning electron microscopes (FIB-SEM)

Highly automated cleanrooms