-Listen to ROHM- ROHM Musical Device MUS-IC

Photo:ROHM Theatre Kyoto

scroll

Culture

IMAGE

For everyone moved by music

ROHM has contributed to popularizing and developing music cultures centering on classic music for more than a quarter of a century with the foundation “Rohm Music Foundation”. As for scholarship assistance for young musicians, we have supported more than 400 young musicians, such as Mr. Daishin Kashimoto, who now serves a concert master at Berlin Philharmonic Orchestra. In addition to that, we host and cooperate for concerts and operas, supporting the comprehensive theatre “ROHM Theatre Kyoto” representing Japan. ROHM, which supports musicians creating music and environments as well as audio fans enjoying music. The IC for music, which is created by our passion and technology for all those who love music. That is ROHM Musical Device “MUS-IC”.

Quality

IMAGE

Everything starts
from quality

Quality, which is the most important for products and has to be mastered with the first priority. In musical instruments, in order to obtain a beautiful and clear tone, an accurate interval and high reliability, the product as a musical instrument must be finished perfectly. ROHM also pursue higher perfection, sticking in the principle of quality first throughout the details of products and declaring “Quality is our top priority at all times.” as a company mission. Only after uncompromising quality lays the foundation, products can prove its real worth, ROHM considers. The IC for the music, which is created by ROHM’s attitude toward the pursuit of quality aiming zero defects. That is ROHM Musical Device “MUS-IC”.

Craftsmanship

IMAGE

In every nook
and corner

Making musical instruments requires proficient skills, deep knowledge and passion. The best musical instrument is finished by this craftsmanship’s infusion throughout all processes of making musical instruments. ROHM adopts the vertical integrated production system that all processes are finished at our site, which is unprecedented in this industry. Each process from pulling silicon ingot up to final packaging handled by engineers with prominent techniques and knowledge makes IC production uncompromising.
Moreover, besides the vertical integrated production system, we use our strong analog circuit technology which has been the foundation of ROHM’s audio IC development over a half-century.
The IC for music, which is created by craftsmanship throughout all processes in the same manner as making musical instruments. That is ROHM Musical Device “MUS-IC”.

Sound

IMAGE

Refine the sound
as it is

Musical instruments cannot be called a true instrument by just finishing its shape. When a piano tuner fully brings power of expression which pianos originally have by adapting them to the best condition, they play a beautiful sound.
In the same manner of this tuning of pianos, the ROHM’s original method “sound quality oriented design” brings the real performance of audio ICs. From among all processes of making ICs from manufacturing wafer to packaging, we abstract 28 parameters which affect sound quality.
Optimizing them one by one with careful listening tests realizes faithful play of fundamental tone drawing the beauty of music as it is. Not just making an electric feature high but making the best quality based, the IC for music, which is refined by the high priority of sound quality in each process of making ICs. That is ROHM Musical Device “MUS-IC”.

From the analog audio era of the 1970s ROHM’s engineers have been dedicated to the development of audio ICs for over half a century.
The resulting vibrations when a player plucks the strings in the tense stillness, the rich bass tones that produce the energetic feel of the sound, someone’s voice touching our heartstrings, and the deep impression they leave when we sense them all over our bodies.
In other words, the above engineers have been aiming to express the view of the world that musicians create.
And in making that dream come true they have pursued both the numerical values and sound quality performance required in an audio device to the utmost limits.
The masterpiece of ROHM audio systems that were created through the ardency of engineers:

ROHM Musical Device MUS-IC

ROHM Musical Device MUS-IC Product Lineup

BD372xx Series

Delivers higher sound quality by providing clean power
The Industry's First Power Supply ICs for High-Fidelity Audio
  • *:ROHM March 20, 2018 study

BD372xx Series

  • Ultra low noise Power Supply ICs most suited for playing high-resolution audio
  • Noise level: less than 5µVrms
  • Ideal power supply symmetry with positive and negative type of power supply ICs
BD3470x Series

Improved spatial representation provides an immersive experience, supporting high-resolution
Sound Processor for High-end AV Amplifers

BD3470x Series (7.1ch),
BD3460x Series
(6ch for automotive)

  • Low distortion (0.0004%) / low noise (S/N ratio -131dB, -125dB) as the industryʼs highest level
  • The original micro step volume decreasing pop noise
  • *:BD3460x Series
BD34301EKV

High performance Audio-DAC applied sound quality design
768kHz sampling, 32bit ⊿Σ Stereo Audio D/A Converter

BD34301EKV(Under Develpoment)

  • Industryʼs top class S/N rate(130dB) and THD+N(115dB)
  • Available for high spec DSD signal (22.4MHz) and PCM signal (768kHz sampling)